Power On and Preset

Power On and Preset ClosedSetup

Power On State

When Line Power Applied

Restore System Settings to Default

Perform Factory Preset

RST Configure

Sets how the instrument should power on and activate certain presets.

GUI Location

System Menu (triple bar icon) > Settings (gear icon) > Power On/Preset

Power On State

Enables you to select whether the instrument powers up in a default state or some other state.

GUI Location

System Menu (triple bar icon) > Settings (gear icon) > Power On/Preset > Power On State

SCPI Command

:SYSTem:PON:TYPE PRESet|USER|LAST

:SYSTem:PON:TYPE?

SCPI Example

:SYST:PON:TYPE PRES

:SYST:PON:TYPE USER

:SYST:PON:TYPE LAST

Preset

This is unaffected by a Preset but is set to Preset on a "Restore System Settings to Default Values".

State Saved

Persistent, survives preset and power cycle but not saved in the instrument state.

When Line Power Applied

This setting determines the action the instrument takes when line power is applied or restored. (For other models, this operation is controlled by settings in the BIOS.)

The choices are:

It is not advised to interrupt line power while the instrument is running by removing the line cord, or switching off a power strip or equipment rack main circuit. The instrument should be shut down gracefully via the front panel power button or :SYSTem:PDOWn SCPI command.

GUI Location

System Menu (triple bar icon) > Settings (gear icon) > Power On/Preset >When Line Power Applied

SCPI Command

:SYSTem:LPRestored:STATe LAST|ON|OFF

:SYSTem:LPRestored:STATe?

SCPI Example

:SYST:LPR:STAT ON

Preset

This is unaffected by a Preset but is set to LAST on a "Restore System Settings to Default Values".

State Saved

Persistent, survives preset and power cycle but not saved in the instrument state.

Restore System Settings to Default

Sets the states that are not affected by signal generator power–on, Preset, or *RST to their factory default settings.

Most settings are affected by Preset, but there are some settings that are unaffected. These are called persistent variables. The system and each application will list its persistent variables. To reset these, select Restore System Settings to Default.

When this control is selected, the following message appears:

"This will reset all persistent variables to their default state. This action cannot be undone. Do you want to proceed?"

The message provides an OK and Cancel button to let you affirm or cancel the operation.

GUI Location

System Menu (triple bar icon) > Settings (gear icon) > Power On State > Restore System Settings to Default

SCPI Command

:SYSTem:PRESet:PERSistent

SCPI Example

:SYST:PRES:PERS

Perform Factory Preset

Sets all states of the signal generator back to their factory default settings, including states that are not normally affected by signal generator power–on, Preset, or *RST.

When selected, the following message appears:

"This will reset all variables (including System variables) to their default state. This action cannot be undone. Do you want to proceed?"

The message provides an OK and Cancel button to let you affirm or cancel the operation.

GUI Location

System Menu (triple bar icon) > Settings (gear icon) > Power On/Preset > Perform Factory Preset

SCPI Command

:SYSTem:PRESet:ALL

SCPI Example

:SYST:PRES:ALL

Notes

No confirmation is required when the SCPI command is sent

RST Configure

Defines whether *RST performs a factory preset or the user preset saved in memory.

SCPI Command

:SYSTem:RST:CONFigure NORMal|USER

:SYSTem:RST:CONFigure?

SCPI Example

:SYST:RST:CONF USER

:SYST:RST:CONF?

Dependencies

Applies only when SCPI Backwards Compatibility Mode is E82x7D. Otherwise, applies NORM, regardless of value. See SCPI Backwards Compatibility Mode.

Preset This setting is unaffected by Preset. It is reset to NORMal on Restore System Settings to Default Values.
Range Normal|User
State Saved Persistent, survives preset and power cycle but not saved in the instrument state.
Backwards Compatibility SCPI

N51xxB

:SYSTem:RST:CONFigure